Hardware connections


Connectors overview

 

System indicators

The Vision Navigator has three LEDs to indicate the current status of the sensor.

 

 

Ethernet connector

Ethernet connector standard

 

 

I/O connector

I/O connector pin overview

 

 

I/O connector pin definitions

Pin

Wire color

Symbol

Description

1

Red

CANH

CAN High #1

2

White

CANL

CAN Low

3

Green

PWR_SHDN

Power shutdown #2

4

Black or Grey

GND

Signal ground

5

Blue

TM_PLS

GNSS1 receiver time pulse

6

Yellow

TM_MRK

Power shutdown #3

7

Orange or Pink

UART1_RX

UART receiver input 1

8

Brown

UART1_TX

UART transmitter output 1

 

#1: A correct CAN network topology is important to avoid CAN communication errors caused by signal reflection or disturbance. The user must ensure proper termination on the CAN bus. The XVN cable must be at most 30 cm to the CAN bus line. If you require a longer cable, you must provide a setup that ensures the integrity of the communication.
#2: When using the I/O connector, the PWR_SHDN pin should be driven low. To shut down the sensor, drive this pin high (3-12 V). The sensor will only restart when the pin is driven low again. This behavior applies to all sensors with version number 1.2A/B or later (refer to the label on the sensor). For sensors with version numbers 1.0 and 1.1, the pin must be driven high during operation (3.3 V) and can be driven low to reset the sensor.
#3: When using the I/O connector, the pin 6 should be driven low.

AUX connector

 

AUX connector pin overview

 

 

AUX connector pin definitions

Pin

Wire color

Symbol

Description

1

Red

+5V

Voltage supply output of 5V

2

White

UART2_RX

UART receiver input 2

3

Green

UART2_TX

UART transmitter output 2

4

Black or Grey

GND

Signal ground

5

Blue

Reserved

Reserved

6

Yellow

Reserved

Reserved

7

Orange or Pink

Reserved

Reserved

8

Brown

Reserved

Reserved

 

 

Power connector

 

Power connector pin definitions

Pin

Wire color

Symbol

Description

1/2

Black

GND

Power ground

3/4

Red

VCC

Main power input

 

 

GNSS connectors

The Vision Navigator contains two GNSS receivers that can connect to an antenna via the female SMA connectors labeled GNSS 1 and GNSS 2.

 

 

WiFi connector

The Vision Navigator can significantly increase its Wi-Fi range by connecting a Wi-Fi antenna to the female RP-SMA connector labeled Wi-Fi.

 

 

USB-C connector

The Vision Navigator contains a USB-C port to connect an external drive for data recording. With firmware version 2.63 and later, the user can also use this port to access the recovery mode (see Sensor configuration).Note that the USB-C port must only be used as a service interface, not during operation.

 

Create your own Knowledge Base