Quick Start


This section is intended to help you install and use the MT Manager quickly. First you need to download the MT Software Suite to your computer. The most recent version of the MT Software Suite can be downloaded from our website. Make sure to download the latest MT Software Suite for MTi products.

 

Installing MT Manager - Windows

For users of previous Xsens’ MT software:

Be sure to uninstall the previous version of the USB converter drivers:

Open the Windows Control Panel and go to Add or Remove Programs.

Look for the entry 'Windows Driver Package - Xsens USB-serial Converter Driver Package'. Please uninstall all entries of these drivers.

 

This installation procedure also tells the procedure to install the entire MT Software Suite. The installation procedure installs several components and starts with the screen as shown below:

 

The installation procedure is straightforward. On the second screen, you can choose to skip installation of several components (not recommended).

 

 

Installing MT Manager - Linux

After downloading the MT Software Suite for Linux, unpack the .tar.gz file to your desired installation folder. Inside you will find, among other components, the file mtmanager_linux-x**_version.tar.gz. Unpack this file also to your desired installation folder.

 

After unpacking, head to ./mtmanager/linux-*/doc/MTM.README to find a list of required packages that need to be installed before you can run MT Manager. Then, go to the ./mtmanager/linux-*/bin directory. In this directory, run the mtmanager executable to start MT Manager (terminal command: ./mtmanager).

 

 

Connecting your device to MT Manager

Connect a device to your PC using the supplied USB cable. With the USB cable, the device is automatically found.

 

Automatic COM port selection

Upon execution of the MT Manager, it automatically scans the available COM-ports and/or industrial motion tracker USB devices on the PC for connected devices.

 

MT Manager scanning for attached devices

 

If you are using an RS-485 sensor, be sure to enable the RS-485 compatibility mode in the General pane via “Tools” -> “Options…”. Without RS-485 compatibility enabled, the RS485 industrial motion tracker device may not be found.

 

The industrial motion trackers are displayed in the Device List with the respective unique MT device ID number.

 

The main screen of MT Manager with an MTi-300 attached via USB

 

After physically connecting one or more devices, press the rescan button  to let MT Manager search for connected devices on any available COM port and update the device list.

When you want to disconnect all devices, press the disconnect button .

 

Manual COM port selection

If you want to select the COM port manually, then in the Connectivity toolbar:

 

The connectivity toolbar

 

You can choose a COM port and the baud rate if you are using a serial connection or a USB converter. See below. Note that the direct USB connection does not have a COM-port. Instead, the USB has a unique USB name that you can find in the Device Settings window () or the Device List .

 

Manually selecting the COM port that MT Manager uses during its scanning procedure

 

Manually selecting the baud rate that MT Manager uses during its scanning procedure

 

For the COM ports, you can choose between all active COM ports. It is recommended to use the “Auto” baud rate to have the baud rate determined automatically. Then, press the “Scan Port” button .

 

Now you are ready to go using your Motion Tracker with the MT Manager.

 

 

Basic functionality of MT Manager

This section describes how to set up the industrial motion tracker for recording and exporting data.

 

Configuring Motion Tracker

After the device is connected, it should show in the Device List in the bar on the left.

 


 

MT Manager showing the MTi-300 with DeviceID 03782083 in the Device List

 

The first step is to configure the industrial motion tracker. Open the Device Settings window .  The Output Configuration settings tab will be shown.

 

The default output configuration can be found in the Low-Level Communications Protocol Document. The preset drop down bar allows choosing other options. Recording data with the XDA processing preset allows reprocessing the file with any compatible filter profile. It is possible to select individual data IDs, but note that when orientation is selected, the onboard processed orientation is recorded. Files with onboard processed orientation data cannot be reprocessed using a different filter profile. 

 

The Output Configuration window features easy to use presets.

 

In this step-through, the settings of the industrial motion tracker other than the output configuration will not be changed. It is, however, possible to change filter settings, configure synchronization options or to review the calibration parameters. In the header, it also shows the hardware ID, Firmware Revision and other device information.

 

The header of the Device Settings window shows general information of the industrial motion tracker.

 

Recording data

First check if you receive data. Open, for example, the 3D view  and the inertial data graph .

 

A typical view of MT Manager

 

Press the record button in the menu bar: .

The record status is shown in the bottom right corner:

Press the record button again to stop recording.

 

Opening the file and playback data

Open the file with File – Open, CTRL+O or the Open File icon . When orientation data is not in the file, a pop-up window will ask for the required filter profile. When applicable, additional processing options can be enabled or disabled by using the check boxes. Refer to your product's  User Manual or Datasheet for more information on filter profiles and additional processing options.

 

After opening a file with MT Manager, a window is shown when orientation is not available in the file.

 

 

You can now playback the file by pressing the Play-button. You can revert to the beginning of the file with the Rewind to Start-button. 

The Playback toolbar

 

Choose to playback data in real-time or at once by changing graph settings in Tools - Preferences.

 

Playback and plotting options

Parameter

Comments

File plotting

Real-time plays data in real-time;

All Data (as fast as possible) plots all data at once. Note that you need to increase the Maximum Display time to see all data;

All Data (update every 5 sec..) is required when the file is extremely large.

Maximum display time

Increase this value to a higher value (File) in order to show more data, especially useful when investigating a file.

 

The Graphs options in the Tools - Preferences window

 

Exporting a file to ASCII

In order to use the data in other programs, e.g. Excel or MATLAB, the MT Manager allows to export the data to a text file. To do so, click open a log file and press the Export button . A window will open in which you can select the data to be exported. When the exported data is not available, the field will be filled with the Empty Field option. Click Export to generate the ASCII text file.

 

The Preferences – ASCII Exporter window

 

Changing MT Manager Color Settings: Light, Dark, and Native mode

Starting from MT Software Suite 2025.5, MT Manager has introduced a new feature that allows users to customize the application’s appearance with selectable color themes. Users can now switch between Light, Dark, and Native (system) modes to match their personal preference or operating system theme. This enhancement improves visual comfort and usability across different lighting environments. The theme setting can be accessed from the Preferences menu under Tools.

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

The UI Theme Style option in the Tools - Preferences window

 

Create your own Knowledge Base