Overview MT Manager

This page describes the options available to the user in the MT Manager.

 


Purpose

The purpose of the MT Manager is to provide easy access to the capabilities of any of the currently supported devices.

The MT Manager can be used to interface with the MT and to visualize and log data. It offers export options for ASCII text files. The ASCII export format can be customised to your needs.

 

MT Manager features

The MT Manager software is an easy-to-use software with a familiar Windows user interface, which allows you to:

 

The MT Manager is therefore an easy way to get to know and to demonstrate the capabilities of your Xsens Motion Tracker.

 

Supported devices

Currently, the following devices are being supported by the MT Manager:

 

For detailed information about these MTs, please refer to the corresponding User Manuals and Datasheets.

Future Xsens Motion Trackers will be supported as of their release.

 

Input Options

The MT Manager can handle real-time input and input from recorded binary files.

 

 

In both cases, the input (file) format is the same.

 

The .MTB log files generated by the MT Manager will contain the following MT messages:

 

The MT Manager software handles the request of these additional data packets from the MT (not only requesting MT Data) to enable full analysis of log-files in the MT Manager software later.

 

NOTE: An MTB file can contain any number of MTData2 packets that are requested from the MT. Only if an MTB file contains Sensor Component Readout or sensor data (∆q/∆v or inertial data) and/or GNSS data messages, the data can be re-processed using different filter profiles. In all other cases, the .MTB file is considered a log-file, which can be played back again for viewing.

In the case that only sensor data and/or GNSS data is requested from the MTi, the MT Manager will run the sensor fusion filter in XsensDeviceApi64.DLL of the host PC (and not on the DSP of the MT) to estimate orientation, position, velocity.

 

Output Files

The MT Manager can export data logged in .MTB files to different formats.

 

ASCII text data

The output orientation can be represented in different conventions:

 

Data and (UTC) time can also be included in the exported files. See Operating Guidelines for more information on the columns of the exported ASCII file.

 

KMZ geographic data

 

KMZ files (available from GNSS/INS data sets only) are excellent to study trajectories in e.g. Google Earth.

 

Menu bar

In the MT Manager menu bar you will find the following entries:

 

The menu bar in MT Manager

 

In the table below, each (sub-) entry is explained.

 

The MT Manager menu structure

Entry (level 1)

Entry (level 2)

Entry (level 3)

Description

File

Open File

 

Open a previously recorded (shortcut: CTRL-O):

  • MT Manager log file (.mtb)
  • Xsens log file (.bin and .xm)
  • Xbus Master log file (.xm)
  • Binary log file (.bin)

Close

 

Closes the currently opened file

Export

 

Export an opened log file to (shortcut: CTRL-E):

  • ASCII formatted file

For more details, refer to Operating Guidelines.

List of last opened files

 

A list of last opened files

Exit

 

Closes MT Manager

View

Displays

Device List

Toggle to open/close Device list.

Message Window

Toggle to open/close the Messages window

Device Settings

Toggle to open/close the MT Settings dialog

3D Orientation

Toggle to open/close the 3D display of orientation

Inertial Data

Toggle to open/close the inertial data graph

Orientation data

Toggle to open/close the orientation graph

Status Data

Toggle to open/close the status graph

Temperature Data

Toggle to open/close the temperature graph

Velocity

Toggle to open/close the velocity graph

Altitude

Toggle to open/close the altitude graph

Device Data View

Toggle to open/close the Device Data terminal

XDA Data View

Toggle to open/close the XDA Data terminal (hidden by default, enable this feature through Tools>Preferences)

Position

Toggle to open/close the position graph

Space Vehicle Information

Toggle to open/close the SV information graph

UTC Date/Time

Toggle to open/close the UTC date/time window

Status bar

 

Toggle to switch on/off the status bar at the bottom of the MT Manager window. This status bar shows playback information, “extended” tool tips etc.

Tools

Preferences

MT Manager

Here you can change the following general settings:

Graphs:

  • Euler Angles (with or without 3σ uncertainty bands) or Quaternions
  • Celsius or Fahrenheit
  • Toggle display graphs as strobes
  • File Plotting mode: Real time or All data
  • Display time in graphs

Miscellaneous:

  • Orientation output frame
  • Toggle show docked MTw’s and log and visualize docked MTw’s
  • Enable RS485 Compatibility
  • Enable XDA Data View

XDA options:

  • Allows to load an alternative filter profiles file ( used by Xsens support department only)

Logging

Here you can change Logging Settings (refer to section Operating Guidelines)

  • Name of the log file (template)

Restore Communication

 

Resets the communication settings of an industrial motion tracker to the default factory settings, allowing you to regain communication with a device in MT Manager (COM port interface only)

Wireless configuration

 

Opens the wireless configuration window (MTw only)

Power off

All Docked MTws

Power off all docked and USB connected MTws

Wireless system

Power off all MTws that have a wireless connection

All Devices

Powers off all MTws

NTRIP Client

 

Opens the NTRIP Client window (refer to Operating Guidelines).

Window

Tile

 

Tiles the open graph windows. Tiling will be done in order of opening. With 3 graphs, opening the graphs in a specific order determines which graph is over the entire height of the window in the left column and which graphs are placed as smaller windows in the right column.

Cascade

 

Cascades the open graph windows

Help

Documentation

 

Links to the latest online documentation

Support

BASE – Knowledge Base and Community Forum

Links to BASE – Articles, guides, FAQ and online user forum

Contact Support

Contact Xsens Product Specialists

Updates

Download Firmware Updater

Links to the download page for the Firmware Updater

Check for new MT Software Suite versions

Check for new MT Software Suite versions

Online Shop

 

Opens the webpage http://shop.xsens.com where accessories and MT’s can be ordered.

About MT Manager

 

Display version information and includes EULA

 

 

Data views, toolbars and buttons

In this section, the sub-windows, toolbars and button functionalities of the MT Manager are explained:

 

 

 The Device List

By default, the Device List is displayed in a sub-window, showing useful information about your MT. Note that the Device List is read only.

The Device List

 

 

The data shown in the Device List

Parameter

Description

Comments

DeviceID

A unique DeviceID. Refer to the Family Reference Manual for an explanation of the DeviceID

Fixed value, retrieved from device

Product Code

Product code, built up from type of device, product series, interface, accelerometer range and gyroscope range.

Fixed value, retrieved from device

Location ID

Location ID that allows identifying the MTi in a system setup

Can be set in Device Settings dialog

Serial Port

USB or COM port number

Automatically detected

Filter Settings Profile

The filter setting profile used for orientation

Can be set in Device Settings dialog.

 

 

The MT System State shown in the Device List

MT System State

Description

Comments

Measuring

The MT is outputting data

 

Recording

Data is being saved to file

 

Flushing

Data is retransmitted after recording has been stopped.

Applies to Awinda MTw only

Config Mode

MT is in config mode. This happens when configuration messages are sent to the MT or when the user puts the MT in config mode.

When you close MT Manager, the device will go into Config Mode. See this article.

File Mode (open)

A file is selected. MT Manager is waiting for the user to process the file.

 

File Mode (loading)

A file is being loaded and processed 

Progress is displayed in the fourth column.

File Mode (ready)

Displayed when a file is loaded and when the entire file has been processed.

 

File Mode (playing)

Displayed when the file is being played back

 

 

With the Device List, it is possible to disconnect specific devices. Right-click on any parameter associated with the industrial motion tracker that needs to be disconnected, right click and choose Disconnect. The device will be removed from the Device List.

 

Right-click on the Device allows disconnecting a single MT

 

The Device List may show a warning sign at the top level and next to the Firmware Revision. Check the tooltip for more information.

Causes for this warning are:

 

Device Settings

In the Device Settings window, several (low-level) settings can be changed, including the output configuration. Take caution in changing settings in Device Settings as these settings can have large effects on the device. In this window it is possible to save and load a set of device-specific settings, including the output configuration that can be copied to other devices (with the same product code). You can always revert a device to its Factory Settings using the Revert button.

 

For details on the Device Settings, please refer to Operating Guidelines.

 

 

Output configuration

In the Output Configuration tab, all output options of the industrial motion tracker can be set, including frequencies and formats.

 

The Output Configuration tab for an MTi-G-710 GNSS/INS. Depending on the device attached, the Output Configuration window may show fewer options.

 

Data Views

The MT Manager offers a wide range of information displayed in its sub-windows, which can be opened and closed via the (Main Views and GNSS) toolbar buttons or the menu bar:

 

The Data Views and GNSS toolbars

 

The individual buttons and their functionality will be explained in the next sub-sections; availability of some of the buttons and related sub-windows depends on the type of the connected device (e.g. position and velocity information will not be accessible with e.g. MTi-20 VRU/AHT or MTi-300 AHRS).

The icons corresponding with the button that activates a specific sub-window are displayed on the top left of each subsection.

 

 3D Box view

The 3D Box View is a real-time graphical (OpenGL) representation of the MT orientation measurements, i.e. roll, pitch and yaw.

 

The 3D Box view is an easy way of visualizing the orientation of any industrial motion tracker.

 

 Inertial data view

Per sensor type, the Inertial Data view graphically shows the 3D calibrated measurement data vs. time:

 

The Inertial data view for acceleration, angular velocity and magnetic field

 

The table below explains the line colours and the buttons in this view.

 

The line colours in the inertial data graph

Colour

Corresponding axis

Red

Acceleration, angular velocity (roll) and normalised magnetic field in X direction

Green

Acceleration, angular velocity (pitch) and normalised magnetic field in Y direction

Blue

Acceleration, angular velocity (yaw) and normalised magnetic field in Z direction

Black

Total acceleration, angular velocity or magnetic field, if available

 

Automatic scaling

It is possible to choose the scaling of the inertial data plot using the pull-down dialog.

 

Tools let you configure the graphs

 

The different scaling options in the graph windows.

Scaling option

Functionality

No auto scaling

Y-scale will no longer be scaled

Expand to fit

Y-scale will be stretched to show all data in the plot.

Full fit

Y-scale will be stretched to show all data in the plot.

 

Zooming

When the Zoom-icon   is selected, you have several options to zoom.

 

Option 1: Press and hold either mouse button, drag mouse to make a zoom rectangle (right button zooms out, left button zooms in):

 

A zoom rectangle in the Euler angles graph

 

 

Option 2: Double click and hold one of the mouse buttons to generate a default zoom rectangle centered around the mouse position with zoom factor 2.0 (right button zooms out, left button zooms in):

Then:

 

Option 3: Use scroll wheel without buttons pressed to simulate a double click centered around the mouse position and immediately applying the zoom i.e. apply a default zoom rectangle centered around the mouse position (right button zooms out, left button zooms in).

 

Note: Zooming is not possible when the autoscale method is set to “full fit”. 

 

Zooming in y-direction only

When zooming with the above option, it can happen that new data will not be shown in the zoom box, as the x-scale (time) ends before the place where new data is created. In order to zoom only in y-direction, enable the function “show all samples” with the show all samples button:

 

When “show all samples” is enabled, the x dimension of the zoom rectangle is always the complete width of the graph:

 

Zooming in y-direction only can be enabled with the button "show all samples"

 

Panning the graph

When the pan icon  is enabled, you can pan the graph with the following actions:

 

Note: Panning is not allowed when the autoscale method is full fit.

 

Panning is available in all directions

 

Showing data values

With the Show Values button  enabled, hovering over the graph will display the values at that moment. 

 

The Show Values button activates the possibility to see the values in the graph

 

 

Showing less data channels

With the checkboxes, it is possible to omit data from the plot. This way, you can closely investigate one particular signal.

Turning off some of the channels allows for closer investigation of a particular signal

 

 

Freezing a graph

When you are using an industrial motion tracker in live view, you cannot pause the file to investigate data further. In that case, you can use the freeze button and zoom and pan on visible data:

 

 

Clearing and resetting graphs

There are two ways of clearing and resetting graphs. To clear the graph, use the clear button .

Another way to reset the zoom that is very convenient when you have used zoom and pan functions, is to close and open the graph.

 

 Orientation data view

The Orientation data view shows the 3D orientation (calculated from the angular velocities) in either Euler angles in degrees vs time or Quaternions vs time

 

The orientation graph shows the orientation of the industrial motion tracker over a period of 10 seconds

 

Starting with MT Manager version 2025.3, and firmware version 1.3.0 or later for Xsens Sirius or Xsens Avior, the orientation uncertainty of the Euler angles can be displayed as a 3σ (three-sigma) standard deviation. This feature can be enabled via Tools > Preferences > MT Manager > Graphs.

 

The orientation graph shows the orientation of the industrial motion tracker with 3σ uncertainty bands.

 

Below table explains the line colours in “degrees vs. time” view:

 

Colours in the Euler angles graph

Colour

Corresponding axis

Red

Roll angle in degrees

Green

Pitch angle in degrees

Blue

Yaw angle in degrees

 

The quaternion graph shows the 4 components in one graph

 

The table below explains the line colours in the “Quaternions vs. time” view:

 

Colours in the quaternion graph

Colour

Description

Red

q1

Green

q2

Blue

q3

Black

q0

 

 Free Acceleration view

The Free Acceleration view window visualizes the 3D Free Acceleration of the industrial motion tracker (VRU/AHT, AHRS and GNSS/INS devices only). By default, Free Acceleration is visualized in the East-North-Up (ENU) format. In order to switch between ENU, NWU and NED visualizations, go to Tools > Preferences > MT Manager > Miscellaneous.

 

The Free Acceleration view, visualizing 3D Free Acceleration in m/s2

 

 MT Status

The MT Status sub-window displays various status flags.

 

Be sure to enable the Status Data Output in MT Output Configuration dialog:

 

Tick boxes for status in the Output Configuration window

 

 

The status window of an MTi-30 AHRS. In this particular screen shot, several gyroscopes are clipping.

 

 

The status windows of GNSS/INS devices can have additional signals, such as GNSS Fix and Filter Mode.

 

 

Signals in the Status window

Colour

Status data description

Red

Motion Tracker has passed the self-test according to eMTS. For an up-to-date self-test indicator, refer to the Low Level Communication Protocol Document, RunSelfTest

Light green

Filter accuracy indicator; low=”not accurate”, high=”accurate”

Dark purple

Manual Gyro Bias Estimation (refer to this article):

 

  • 1 (high): Running with no rotation assumption
  • at 2/3 of the y-axis: Error: rotation detected, no gyro bias estimated
  • 0 (low): Estimation complete, no errors

Bright blue

GNSS fix; indicates if the GNSS receiver has a valid fix

Dark red

RTK fix:

  • 1 (high): RTK fix
  • at 1/3 of the y-axis: RTK float
  • 0 (low): No corrections applied

Orange

RepMo: Representative Motion mode of In-run Compass Calibration (ICC) active

Dark blue (3x)

Clipping flags for the accelerometers, 20g

Dark green (3x)

Clipping flags for the gyroscopes, 450 deg/s or 1000 deg/s

Brown (3x)

Clipping flags for the magnetometers

Magenta

Filter mode; indicates what the state of the filter in the GNSS/INS device is. Refer to the Low Level Communication Protocol Document for details.

 

 Temperature view

The Temperature view window shows the internal temperature of the device. Temperature data is visualized in degrees Celsius by default. In order to change to degrees Fahrenheit, go to Tools > Preferences > MT Manager > Graphs.

 

The Temperature view window, showing that the device is warming up directly after powering it.

 

 Heave view

The Heave view window displays the heave data from the device (Avior/Sirius devices only). The data is visualized in two forms: heave position, shown in centimeters (cm), and heave period, representing the duration of the heave cycle.

 

The Heave view window, showing both position and period data.

 

 

 Velocity view

The Velocity view window visualizes the 3D velocity of the MTi (GNSS/INS devices only). By default, Velocity is visualized in the East-North-Up (ENU) format. In order to switch between ENU, NWU and NED visualizations, go to Tools > Preferences > MT Manager > Graphs.

 

The Velocity data view, displaying 3D velocity in m/s

 

 Altitude view

The Altitude view window visualizes the altitude of the MTi (GNSS/INS devices only). Altitude is displayed as height above the WGS-84 Ellipsoid in meters.

 

 

The Altitude data view, displaying height above the WGS-84 Ellipsoid in meters

 

 Position view

The Position view window visualizes the 2D position of the MTi (GNSS/INS devices only). Position is displayed in terms of longitudinal and latitudinal coordinates.

 

 

The Position view, displaying 2D position

 

 Space Vehicle Information window

The Space Vehicle Information (or SatInfo) Window shows the various satellites with their respective signal strength in dBHz.

 

The columns are labelled according to the constellation and the number of the space vehicle. The digit in front of the semicolon indicates the satellite system, the number after the semicolon is the satellite number. E.g. 0:5 indicates Space Vehicle #5 from the GPS constellation. The labels are described in the table below.

 

Colours used in the SV information window

Label

Color

Meaning

Detected (unused)

Blue

The satellite data is not used for the navigation solution.

Note that SBAS satellites (1:#) can only be detected or unhealthy. If SBAS corrections are being used for the GPS satellites, the GPS satellites are light green.

Used

Dark green

The satellite data is used for the navigation solution. No differential corrections have been applied.

Used+D

Light green

The satellite data is used for the navigation solution and differential corrections have been applied.

Unhealthy

Red

The satellite data is not used.

 

 

The SV info window showing 5 GPS satellites and 6 GLONASS satellites being used for the navigation solution and 2 satellites that have been detected.

 

 UTC Time view

The UTC Time view window visualizes the UTC Time output of the industrial motion tracker. The GNSS receiver automatically retrieves UTC Time for the GNSS/INS devices. For all other devices, UTC Time can be set manually (see Operating Guidelines).

 

The UTC Time view.

 

 Device/XDA Data View terminals

The message terminal shows messages sent to and received from the device or the Xsens Device API (XDA) in real-time. The Device Data View terminal can also be used to compose low-level messages in order to quickly understand the communication protocol. See Operating Guidelines for more information about the message terminals. The XDA Data View is hidden by default. It can be enabled through Tools>Preferences.

 

The message terminals for the device (left) and XDA (right)

 

Message window

The message window shows warnings and other informational messages.

 

The message window may show warnings on e.g. missed data packets

 

Connectivity

With the Connectivity toolbar, you can control connecting your devices:

 

The Connectivity toolbar

 

Please refer to Quick Start for details on how to connect and disconnect your devices.

 

 

File control

The file control tool bar makes it possible to choose where files are stored and opened.

 

The File control toolbar

 

 

Meaning of buttons in the File Control toolbar

Icon

Action

Open a previously recorded file (see also “File -> Open…”)

Export an opened log file (see also “File -> Export…”)

Set the Current Directory (by browsing)

 

 

Playback & recording

To be able to record data and playback recorded data, the MT Manager offers the Playback & Recording toolbar.

 

    

The Playback and recording bar when an industrial motion tracker is attached (left) and when a file is loaded in MT Manager (right)

 

Meaning of the buttons in the Playback and Recording toolbar

Button name

Button icon

Functionality

Record/

Stop Record

Pressing this button will turn on the logging of data to a file (see also Operating Guidelines)

Releasing this button in recording mode will turn off the logging

Play

Pressing this button will start (or continue) playback of logged data (see also Operating Guidelines)

Rewind

During playback, pressing this button will go to the start of the logging

 

 

 

Orientation resets

 

Please refer to BASE - Changing or Resetting the MTi Reference Coordinate Systems for detailed information about orientation resets and the effects these have. Available resets are summarized in the table below.

 

The available orientation resets

Reset type      

Functionality

Heading reset

redefines North to the x-axis of the device – applies to RotLocal

Inclination reset

redefines device coordinate system such that momentary inclination is zero – Applies to RotSensor

Alignment reset

combines the heading reset and the object reset – applies to both RotLocal and RotSensor

 

After choosing the reset type, press the Reset Orientation button .

 

You can also choose to apply the reset on the current device or on all connected devices.

After a reset, you can store the new values to the MT Settings by pressing the Store Orientation button .

 

The orientation resets toolbar can be used to apply a specific reference coordinate system to the device's orientation, velocity and sensor data output.

 

 

In-run Compass Calibration & Representative Motion

In-run Compass Calibration is a way to calibrate for magnetic distortions present in the sensor operation environment using an onboard algorithm, leaving out the need for a host processor like a PC. It estimates the hard- and soft-iron effects and provides new magnetometer calibration parameters. To expedite the calibration of the magnetometer sensor readings with respect to the new field, there is a feature called Representative Motion. Click the button Start/Stop Representative Motion and rotate the device together with the object that disturbs the magnetic field in all directions of the actual application.

 

Click the Representative Motion button to start the Representative Motion mode. Click it again to stop the Representative Motion mode.

 

If you want to store the new values in the non-volatile memory (remember that they are discarded when you power cycle the industrial motion tracker), press the store button:

 

This button stores the ICC parameters in the non-volatile memory

 

For more information on ICC and Representative Motion, refer to the following link on BASE: In-run Compass Calibration (ICC) and Representative Motion

 

 

Manual Gyro Bias Estimation

Manual Gyro Bias Estimation is a way to quickly estimate the gyroscope zero-rate offsets or biases. This feature can be particularly useful when trying to reduce Yaw drift with VRU/AHT devices or slowly moving GNSS/INS devices. Manual gyro bias estimation forces the filters of the industrial motion tracker to estimate the gyroscope biases by assuming that the device will be held motionless for a given period of time.

 

In order to perform a manual gyro bias estimation using MT Manager, click the corresponding icon, . A window will open, providing guidelines for the user. For more information on this feature, refer to BASE: Manual Gyro Bias Estimation

 

The Manual Gyro Bias Estimation window guides the user through the use of the feature.

 

 

Create your own Knowledge Base