Please note that all products within the MTi-10 series, including -O and -DK versions, have reached their End-Of-Life date. The MTi-10 series has effectively been replaced by the new MTi 600-series. For further information, please refer to the Product Change and EOL Notices chapter, specifically MTi-10 EOL Notice.


Stresses above Absolute Maximum Ratings may cause permanent damage to the device.
| Shock (any axis) | 20000 m/s2 (2000 g) 0.5 ms (half-sine) |
| Input Voltage | -60 V … 34 V |
| Alternative Input Voltage | 3.3 V +/- 0.1 V |
| ESD | 8 kV; above 2 kV possibility of data loss and/or temporary connection loss |
| Interface inputs |
-25 V … 25 V (RS232 RX) -11.7 V … 15 V (RS422, RS485 A and B inputs) -0.3 V …3.6 V (alternative UART) |
| SyncIn | 0 – 20 V |
| Operating/Storage Temperature | -40 °C … 85 °C |
| Humidity | Casing is IP67 (for OEM: 95% max, non-condensing) |
Stresses beyond those listed here may cause permanent damage to the device. Exposure to absolute maximum rating conditions for extended periods may affect device reliability.
NOTE: Drops onto hard surfaces can cause shocks of greater than 20000 m/s2 (2000 g) exceed the absolute maximum rating of the device. Care should be taken when handling to avoid damage. Drops causing shock greater than absolute maximum ratings may not destroy the device but will permanently alter the properties of the physical motion sensors, which may cause the device to become inaccurate.
The MTi will not require any maintenance if properly used. However, if the Motion Tracker is not functioning according to the specifications, please contact Xsens or your local distributor (www.xsens.com/support).



Xsens Technologies B.V. warrants the products manufactured by it to be free from defects in material and workmanship for a period of two years from the date of delivery. Products not subjected to misuse will be repaired, replaced or credit issued at the sole option of Xsens Technologies B.V. Contact Xsens via www.xsens.com/support for return material authorization (RMA) prior to returning any items for calibration, repair or exchange. The product must be returned in its original packaging to prevent damage during shipping.
The warranty shall not apply to products repaired or altered or removed from the original casing by others than Xsens Technologies B.V. so as, in Xsens Technologies B.V. opinion, to have adversely affected the product, products subjected to negligence, accidents or damaged by circumstances beyond Xsens Technologies B.V.’s control.
NOTE: Xsens reserves the right to make changes to its products in order to improve design, performance, or reliability.
Subject to the conditions and limitations on liability stated herein, Xsens warrants that the Product as so delivered shall materially conform to Xsens’ then current specifications for the Product, for a period of one year from the date of delivery. ANY LIABILITY OF XSENS WITH RESPECT TO THE SYSTEM OR THE PERFORMANCE THEREOF UNDER ANY WARRANTY, NEGLIGENCE, STRICT LIABILITY OR OTHER THEORY WILL BE LIMITED EXCLUSIVELY TO PRODUCT REPAIR, REPLACEMENT OR, IF REPLACEMENT IS INADEQUATE AS A REMEDY OR, IN XSENS' OPINION IMPRACTICAL, TO REFUND THE PRICE PAID FOR THE PRODUCT. XSENS DOES NOT WARRANT, GUARANTEE, OR MAKE ANY REPRESENTATIONS REGARDING THE USE, OR THE RESULTS OF THE USE, OF THE PRODUCT OR WRITTEN MATERIALS IN TERMS OF CORRECTNESS, ACCURACY, RELIABILITY, OR OTHERWISE. Xsens shall have no liability for delays or failures beyond its reasonable control.